Business Recovery:

Products and solutions to help your business move forward.

Get Started

Safety & Health

Electrical Hazard Safety

Insulated Hand Tools

2/3/19
Quick Tips #204

Insulated hand tools play a role in creating a safe workplace for employees who are working near energized circuits

Whether they're high in the sky working on power lines, elbow-deep in a generator, or re-wiring a critical piece of control equipment on the factory floor, electrical workers need tools that are designed and engineered for maximum safety.

Because insulated tools and energized environments go hand-in-hand, there are some key points to keep in mind when buying, using and retesting such tools. Here's a look at some of the most important:

Buying and Using Insulated Hand Tools

Used to protect workers working live or close to live parts against arc flash, arc blasts and electrocution, insulated tools are rated at 1,000 volts AC (and 1,500 volts DC), but are subjected to 10,000 volts during the product testing process (as mandated by ASTM F1505). Hand tools covered by ASTM F1505 include screwdrivers, wrenches, pliers, nippers, strippers, cable cutting tools, cable scissors, knives and tweezers.

Complying both with the National Fire Protection (NFPA) 70E® and the International Electrotechnical Commission (IEC) 60900 standards, insulated tool sets are individually tested and certified by the manufacturer for specific working conditions.

When purchasing insulated hand tools, safety directors should seek out those that comply with IEC, ASTM, and/or the Deutsches Institut fur Normung (DIN) standards. While these groups do not test the individual tools for compliance (manufacturers do their own testing), they do set the insulation performance requirements for the tools.

The Verband der Elektrotechnik, Elektronik und Informationstechnik (VDE), the association of German electro technicians, is an independent agency that tests a sample of each tool to ensure compliance.

To increase tool life and ensure that the insulated hand tools provide protection for users, be sure to:

  • Keep tools clean and dry
  • Inspect insulation before each use
  • If you doubt the integrity of the insulation, destroy the tool or have it retested
  • Follow the manufacturer's temperature recommendations for use
  • Have a qualified person inspect and recertify tools annually for safe use
  • Use other personal protective equipment as necessary

Retesting Hand Tools

Although there aren't specific requirements for retesting insulated hand tools, in compliance with 29 CFR 1910.335(a)(1)(ii), protective equipment must be maintained in a safe, reliable condition. Most manufacturers suggest inspecting the insulation before each use and having a qualified person perform an annual inspection and certification. To aid in the inspection process, some manufacturers offer two-layer insulation that will change color when the insulation has been breached.

When using insulated tools, make sure workers always follow the manufacturer's recommendation. Although insulated hand tools are tested and certified to 1,000 volts AC, the testing agencies do not recommend using them on energized circuits, for example, and most insulating tools are designed only for protection from accidental contact with energized circuits.

 

The information contained in this article is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This article is not a substitute for review of current applicable government regulations, industry standards, or other standards specific to your business and/or activities and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

SIGN UP FOR EMAIL

Get more great content like this sent to your inbox.

promo

THE PRODUCTS YOU NEED,
WHEN YOU NEED THEM

SHOP NOW