Industry

Manufacturing

Guiding the Automated Guided Vehicles Industry

11/14/17
Industrial Maintenance & Plant Operation • Jonathan Wilkins

Automated guided vehicles are mobile robots that follow markers or signals during navigation. The first AGV was introduced in the 1950s by Barrett Electronics and performed a simple towing action, with its position guided by a wire in the floor. Since the 1950s, the market has rapidly increased, and AGVs are used across numerous industry sectors.

Why AGVs?

Automated guided vehicles are predominantly used for materials-handling purposes. This can include a range of tasks, from on-time delivery of parts to the production line to round-the-clock transit. If the vehicle is equipped with a clamping mechanism, positioning fixtures and tool attachments, it can perform a range of functions.

Depending on the application and requirements, AGVs can function in isolation or in fleets. This makes the use of AGVs scalable according to need, so a plant manager can make a specific decision on the number of vehicles in a facility.

AGVs can be equipped with sensors for traceability, so that the plant manager can monitor the position of each individual vehicle and therefore track the movement of materials around a facility. Pick-up, transit and delivery of items can be time-stamped as part of this process to further improve tracking. This information can be integrated into the company’s enterprise resource planning (ERP) or materials resource planning (MRP) systems.

Depending on the application, there are different types of vehicle navigation methods. A plant manager can opt for a very simple system, similar to the earliest AGVs, or can choose more advanced navigation methods.

Navigate

The earliest AGVs were guided around the factory by a wired method. To navigate in this way, a wire is embedded into a slot in the floor and transmits a radio signal, which can be detected by a sensor on the AGV. The AGV is then guided around the facility following the wire. Though this navigation technique is still used today, there are a variety of other methods for plant managers to choose from.

Some AGVs use guide tape that is either magnetic or colored to navigate. Sensors on the AGVs detect the tape, and this is used to guide the vehicle. Guide tape is also used in laser-target navigation, where reflective tape is mounted on walls, poles or machines and the AGV calculates distance using a laser transmitter and receiver. This has an advantage over the wired method, because it is easier to change the route of the vehicle as the process of relocating the tape is more straightforward.

In inertial navigation, reference points are embedded into the factory floor at X-Y coordinates. The AGV uses information from a sensor, a gyroscope and a wheel encoder to determine location. Changes can be made to the pathway by simply altering the reference points, making this method more flexible. However, some change to factory infrastructure is still required, and the vehicle cannot make independent route-planning decisions.

The next step from inertial navigation is open path navigation -- this means the vehicle can move independently from one place to another, moving from a guided vehicle to a self-driving vehicle.

From Guided To Self-Driving

Traditional AGVs perform defined, pre-programmed movements around a facility. This means there is some difficulty changing the vehicle’s route once specific infrastructure is in place. Recently, more flexible and intelligent vehicles have been introduced, which are able to make decisions in situations that they haven’t encountered before.

This new breed of vehicle can overcome one of the key problems for AGVS -- encountering something unexpected. In a changing environment, a self-driving vehicle may be a better fit. This type of vehicle operates independently from a driver or a fixed pre-programmed input directly controlling the steering, acceleration or braking. Laser-based perception and navigation algorithms can be used to dynamically navigate around a factory.

An on-board programmable logic controller (PLC) can be integrated to reduce errors and make decisions. By connecting to the central control system, the vehicle can analyze the reliability and efficiency of its routes and adapt them accordingly. The vehicle can use machine learning to be more efficient across new situations.

Self-driving vehicles can use an on-board computer and increased numbers of sensors to complete more complex tasks, including decision-making. Independent and intelligent navigation methods can even mean the plant manager does not need to modify factory environment or infrastructure. One such navigation technique is natural feature guidance, where the vehicle can record and store images and calculate its position in relation to existing features.

An example of an autonomous AGV is Clearpath Robotics’ OTTO, a self-driving vehicle that can move up to 3,300 pounds at 4.5 mph. OTTO can adapt to take the best route, avoiding collisions as it moves.

The vehicles can also use vision-based guidance systems, using cameras to act as eyes. An additional benefit of this is that plant managers gain a 3D, virtual view into the environment the equipment is operating in. This means if the AGV does come across anything unplanned or unusual, the operator can easily find the explanation and correct it.

As more factories are upgraded and new facilities are built, advancing AGVs will prove to be a core component of the smart factory. With improving sensor technology and increasing autonomy, AGVs are becoming smarter and more dynamic, moving from guided vehicles following a set path to autonomous independent decision makers -- much like Konrad’s animals will as they grow.

SIGN UP FOR OUR EMAIL NEWSLETTER

Stay ahead of the curve with industry insights and news you can use.

promo

THE PRODUCTS YOU NEED,
WHEN YOU NEED THEM