Industry

Food & Bev

Ensuring Dusty Ingredients Don't Become a Powder Keg


Food Manufacturing

When most people consider the fire hazards in their homes, they probably don't think about the dry ingredients like flour, sugar and corn starch sitting in their kitchen pantry. However, for food manufacturers working with large volumes of dry ingredients, dust-related combustibility is a cause for concern. Food products account for a significant percentage of combustible dust-related incidents in manufacturing, and it is important to be aware of these hazards in your specific line of business.

We had a chance to speak with Caitlin Lucia, senior process engineer, Global Engineering, Campbell Soup Company, regarding dust mitigation in food manufacturing. 

How important is the subject of dust-related combustible hazards in food processing?

Unfortunately, these hazards are generally not as well recognized as they should be, but they constitute a serious safety concern for manufacturers and their employees. They can also be a potential hazard for the communities surrounding production facilities. An in-depth study by the U.S. Chemical Safety Board (CSB) in 2006 identified 281 combustible dust-related incidents between 1980 and 2005 that killed 119 workers and injured more than 700. Food products accounted for nearly a quarter of all the incidents. Beyond the human toll, such events can result in catastrophic costs to facilities and equipment.

What are some key issues that processors need to be aware of?

Equipment owners and end-users must first of all be aware of the hazards specific to their dry ingredients, and with their equipment. Not all dry ingredients are the same; similar food products for taste, texture or powder behavior can have very different propensities for producing a combustible dust explosion. For example, two food starches can have wildly different dust deflagration properties because of chemical composition, particle size and moisture level.

What steps do manufacturers need to take to reduce their risk?

After understanding the risks associated with ingredients that you handle, the next step is to evaluate your equipment and management systems for compliance with the standards. A significant number of food manufacturing facilities were built several decades ago. The age of the equipment in many cases does not exclude manufacturers from the Occupational Safety and Health Administration (OSHA) General Duty Clause, or from standards set by the National Fire Protection Association (NFPA). If you have older equipment that lacks protection from combustible hazards, it's your responsibility to address the risk.

Are there special considerations for food manufacturers that don't affect other industries?

Food manufacturers need to ensure that any powder handling equipment or explosion protection devices are considered for food safety implications. For example, equipment installed in food production areas may need to be compatible with wet wash downs, and materials of construction should be evaluated for potential contamination risks. Similarly, explosion venting systems that mitigate combustion risks should be designed with potential sources of contamination from insects, birds and weather in mind. These are considerations that don't impact other industries to the extent they do food manufacturers.

What should food manufacturers consider when seeking guidance from third parties?

When looking for an equipment vendor, engineering firm or systems integrator, it's important to verify their familiarity with NFPA standards, which are regularly updated. For example, there were several significant changes in the 2017 revision of NFPA 61, the standard geared toward food manufacturing facilities. It's important that your consultants stay on top of these changes. Generally, engineers and vendors who regularly work with powder handling equipment have a solid understanding of the latest standards and guidelines.

This article was from Food Manufacturing and was legally licensed through the NewsCred publisher network. Please direct all licensing questions to legal@newscred.com.

SIGN UP FOR OUR EMAIL NEWSLETTER

Stay ahead of the curve with industry insights and news you can use.

promo

THE PRODUCTS YOU NEED,
WHEN YOU NEED THEM