Industry

Commercial

Seven Tips to Drive Productivity with Ergonomics

5/7/18
Industrial Maintenance & Plant Operation • Brian Neuwirth

In any work environment, as noise and activity levels increase, the risk of danger also increases. In a busy warehouse environment, filled with conveyors, forklifts, rack systems and other moving parts and multiple shifts running at high volumes, the danger of serious workplace injury or even fatality is a very real possibility. From distracted workers to defective equipment to deadly premises violations, workplace accidents are distressingly common, and not just of the slip-and-fall variety.

In 2014, approximately 3 million workplace injuries were reported by private industry employers to the U.S. Bureau of Labor Statistics. These injuries have a staggering financial impact upon the operations and facilities where the injury takes place. ​​According to the 2016 Liberty Mutual Workplace Safety Index, the most disabling, nonfatal workplace injuries amounted to nearly $62 billion in direct U.S. workers compensation costs. These costs can easily cripple an operation.

According to the Joint & Bone Initiative, “70 percent of persons reporting bed and lost work days reported having a musculoskeletal condition. This is more than twice the proportion reporting depression, the second most common medical condition listed for causing lost work days, and five or more times the proportion for other major health conditions. Overall, the high proportion of workers reporting lost work days or bed days as a result of a musculoskeletal condition results in an economic burden on the economy — much higher than that reported for chronic circulatory or chronic respiratory conditions.”

When it comes to the material handling industry, back injuries are one of the most common issues reported by facilities. Per the Bureau of Labor Statistics, back injuries accounted for 19.6 percent of 905,690 injuries referenced in the private sector, higher than the hand, which is 13.4 percent, and shoulder, which is 7.5 percent. The total time lost to work-related injuries in 2013 was 60 million days, and another 35 million years of productive time was lost the same year because of permanently disabling injuries that had occurred in prior years.

Lifting and moving equipment, pallets and boxes in the warehouse can lead to fatigue and injury, especially when the worker performs the task repeatedly or for long periods of time. The National Safety Council reports that these injuries occur because of “awkward postures, repetitive motions, forceful exertions and static postures.”

Musculoskeletal disorders can be prevented by implementing solutions that reduce the need for the worker to reach awkwardly or to overexert themselves.

Ergonomics Is The Answer

Ergonomics is the science of designing the job to fit the worker instead of physically forcing the worker’s body to fit the job. It lessens muscle fatigue, increases productivity and reduces the number and severity of work-related musculoskeletal disorders.

Eliminate unnecessary manual lifts by incorporating simple lifts, using carts and conveyors or implementing carton flow systems to move boxes or items. Carton and gravity flow systems install easily into existing pallet racks, helping to create ergonomic workstations ideal for picking, assembly or line side storage.

Make sure employees stand correctly and use safe lifting techniques. Test the weight and stability of the item to be lifted before lifting to make sure things won’t shift unexpectedly, throwing the worker off guard and leading to possible injury. If the load is unstable, it may need to be repacked.

When lifting items, get a secure grip using both hands, if possible. Keep the load in the “golden zone,” which is above the knees, below the shoulders and close to the body. Use the legs to lift the load; not the back or shoulders. Don’t twist body; instead, step to one side to turn.

If a case is stored on a pallet on the floor, workers have to bend and reach, limiting their ability to properly lift the case and increasing their odds for injury. If the case is stored deep within a pallet rack, visibility and reach is compromised and further jeopardizes the worker’s safety when picking a case. Using pallet racks with rollers or that are tilted so when a box or pallet is removed, the next one to pick moves forward, eliminating the need for stretching and reaching is best for minimizing injury. Making sure products are at the point of pick so workers don’t have to climb into the pallet rack makes lifts easy and safer.

OSHA provides these seven steps of an ergonomic process:

1. Provide management support, with a strong commitment by management being critical to the overall success of the process.

2. Involve workers in hazard assessments, solution development and also implementation.

3. Provide training so that workers are aware of ergonomics’ benefits and will know why is it important to report early symptoms of MSDs.

4. Identify ergonomic problems in the workplace before they result in MSDs.

5. Encourage early reporting of symptoms, which is important for preventing serious injuries and lost-time claims.

6. Implement solutions to control the hazards.

7. Evaluate your progress periodically to ensure continuous improvement and long-term success.

The focus on ergonomics doesn’t just help prevent injury, it maximizes employee output and productivity. Choose solutions that are built with worker safety in mind, allowing your operation to run smoothly while increasing efficiency.

SIGN UP FOR OUR EMAIL NEWSLETTER

Stay ahead of the curve with industry insights and news you can use.

promo

THE PRODUCTS YOU NEED,
WHEN YOU NEED THEM