Business Recovery:

Products and solutions to help your business move forward.

Get Started

Industry

Commercial

How to Comply with OSHA's Silica Construction Rule


Grainger Editorial Staff

A final rule by the Occupational Safety and Health Administration (OSHA) is now in place to curb lung cancer, silicosis, chronic obstructive pulmonary disease and kidney disease in America’s construction workers by limiting their exposure to respirable crystalline silica.

Approximately 2 million construction workers that drill, cut, crush or grind silica-containing materials like concrete, quartz, and stone are exposed to respirable crystalline silica. Another 300,000 workers in brick manufacturing, foundries, and hydraulic fracturing also are exposed to breathing the material, which in severe cases can be disabling and fatal. The respirable silica enters the lungs and creates scar tissue, reducing the ability to take in oxygen.

According to OSHA, the most severe exposures for construction workers arise from the use of abrasive blasting with sand to remove paint and rust from bridges, tanks, concrete structures and other surfaces. Other activities that may result in severe exposure include jackhammering, rock/well drilling, concrete mixing, concrete drilling, brick-and-concrete block cutting, and tunneling operations.

OSHA’s final rule reduces the permissible exposure limit for respirable crystalline silica to 50 micrograms per cubic meter of air over an average eight-hour shift. To comply with the rule, OSHA urges employers to use engineering controls that limit worker exposure, provide respirators when engineering controls fail to adequately limit such exposure; and train workers on silica risks, among other guidance. The rule becomes enforceable for construction entities on June 23, 2017.

Risks of Noncompliance

The health hazards of respirable crystalline silica were initially highlighted by the U.S. Department of Health in the 1930s, after an outbreak of worker deaths rang alarm bells. In 1971, when OSHA was created, the department established its initial exposure standards. These benchmarks have since been deemed inadequate to protect workers from silica-related diseases. In addition, workers are being exposed to respirable silica in industries that did not exist in the 1970s, such as companies engaged in the construction of stone countertops.

“OSHA has long been of the opinion that the widespread use of this material in construction activities is a hazard affecting many workplaces,” said Nickole C. Winnett, an attorney specializing in OSHA cases at the law firm of Jackson Lewis in Reston, Virginia. “Almost 700 deaths are attributable to silica exposure each year, despite what OSHA sees as a pretty easy fix — engineering controls and work methods that reduce exposure and save lives.”

For many construction firms, management must balance the need to protect workers and remain compliant with OSHA’s final rule, while also improving operating efficiency, reducing expenses and increasing productivity. A challenge is overreliance on workers to take actions limiting their exposure to workplace hazards. A recent survey of more than 150 safety, plant and human resource managers by Ansell indicated that 87 percent of employees at the respondents’ organizations were noncompliant with the companies’ personal protective equipment rules, such as the requirement to wear safety hats and goggles.

Although company leaders, and especially supervisors and foremen, need to enhance their oversight of hazard safety practices, management must also ensure that employees understand the ramifications of noncompliance. “Construction companies that fail to adhere to the final rule on respirable silica will be issued a citation at a cost of at least $12,000 for serious offenses,” said Winnett. “If the government believes a company has willfully violated the regulation, the penalty could be well over $70,000 per incident.”

The financial damages pale when compared to the reputational repercussions, she asserted. “The Obama administration used noncompliance with OSHA as a public ‘shaming’ tool, actually listing serious violators on a ‘wall of shame’ to induce them to take responsible actions,” said Winnett. “The Trump administration will likely do less of this. But one can expect the media to pick up the slack, resulting in the loss of potential contracts for a construction company if its operations are portrayed as being unsafe for workers.”

Taking Strong Actions Now

In their preparations for the new rule, Winnett advised that construction firms first review the current engineering controls they have in place. “They should already be in the process of implementing controls, primarily some type of exhaust ventilation system or a wet cutting alternative method to dry cutting processes to reduce the volume of silica in the air,” she said.

Other actions include the possible replacement of crystalline silica materials with safer substitutes, the use of water spraying to control airborne particles, the wearing of disposable work clothes and the vacuuming of a worker’s clothes upon leaving the worksite. OSHA further recommends that construction employees not eat, drink, smoke or apply cosmetics at a worksite where crystalline silica is present, and thoroughly wash their hands, faces and other exposed body parts upon leaving the site. Regular routine medical screening of workers is also advised.

“Companies must make sure that in situations where wearing a respirator is required, workers wear only certified equipment like N95 NIOSH respirators and Type CE abrasive-blast supplied-air respirators in abrasive blasting situations,” said Winnett, noting that sheer dependence on respirators is not a compliance cure-all. “OSHA says construction firms must first rely on engineering controls, resorting to respirator use only under certain circumstances where the hazards are acute,” she explained.

Above all, employers are urged to ensure their employees participate in training programs that focus on the adverse health outcomes of crystalline silica exposure and the various methods to reduce the hazard. “Training is the number one best practice,” said Winnett. “If employees understand the specific hazards that exist and why there are controls, policies and procedures in place, they’ll be more apt to comply with the rule.”

She added that supervisors, and especially foremen, also should be required to attend classes on exposure-reduction methods.

“We’re working with our clients to ensure they have put together written safety plans, providing them with a checklist we developed of what needs to be done, since OSHA does not have a template,” said Winnett. “It lists each type of job in the construction sector with a ‘check-the-box’ series of controls and respirators currently in use. It’s just a simple spreadsheet, but it makes it a lot easier for supervisors and foremen to be certain of their workers’ compliance.”

With June 23 right around the corner, time is of the essence.