Business Recovery:

Products and solutions to help your business move forward.

Get Started

Equipment

Portable Air Conditioner Guide

5/5/21
Grainger Editorial Staff

Portable air conditioners can be a good temperature-control solution in places where HVAC systems are inadequate or nonexistent. Portable AC units can help keep hard-to-cool areas comfortable for people working or living in them, they can help maintain safe operating temperature for heat-sensitive equipment, and they can be moved from place to place as needed.

There are two basic kinds of portable air conditioner:

Light-Duty Portable Air Conditioners

Light-duty portable air conditioners are designed to cool rooms in offices, schools and homes. They're similar to window air conditioners, but they're generally more expensive to buy and to operate. For this reason, light-duty portable air conditioners are most commonly used in places where it isn't possible to install a window AC. Here are some places where portable air conditioners are frequently used:

  • In rooms that don't have the right kind of windows. Most window air conditioners can't be used in sliding windows and casement windows that swing outward.
  • In buildings that have rules forbidding window air conditioners. For example, some commercial landlords and homeowners' associations may not allow window AC installation.
  • In windows that have security bars or features that prevent air conditioner installation.

A common misconception about portable air conditioners is that they can be used without access to a window, but in many cases this is not true. Light-duty portable AC units have an exhaust hose that must be connected to a window or unconditioned space, and some dual-hose models have an intake hose that connects to the window or unconditioned space as well.

Some heavy-duty portable air conditioners are designed to provide spot cooling in large spaces without access to windows for ventilation, but these machines, used in industrial facilities, information technology settings and other special purposes, would not be practical or effective in normal office and residential settings, except in special circumstances. For example, a heavy-duty portable air conditioner might be used to cool an office space when its primary air conditioning system is not working.

Cooling Capacity: ASHRAE vs. SACC

Light-duty portable AC manufacturers often provide two ratings of cooling capacity:

  • The ASHRAE rating, which gives cooling capacity in Btu per hour using an older testing standard developed by the American Society of Heating, Refrigerating and Air-Conditioning Engineers.
  • The SACC (seasonally adjusted cooling capacity) rating, which gives cooling capacity in British thermal units per hour (BtuH) using a newer, more thorough testing standard that was put in place in 2016.

While both ASHRAE and SACC ratings describe performance in BtuH, the SACC rating will be lower than the ASHRAE rating for the same appliance because of the differences in testing procedure. Many portable air conditioner manufacturers include both the ASHRAE rating and the SACC rating.

While these cooling capacity ratings can be used to compare the power of one portable AC unit to another, they can be misleading when comparing the power of a portable AC unit to that of a window AC unit, even though both will be rated in BtuH. The problem is that different test conditions are used for the two categories of air conditioner. (Energy efficiency test procedures for air conditioners are developed by the Department of Energy.) In practice this means that a portable unit rated at 10,000 BtuH may not have the same cooling power as a window unit rated at 10,000 BtuH, for example.

Fortunately, there's an easy way to get around this. When sizing a portable air conditioner, don't rely on sizing charts or formulas designed for window units. Instead, consult the manufacturer's guidance on how much space a specific unit can be expected to cool.

Energy Efficiency: CEER and EER

The combined energy efficiency ratio (CEER) is a measure of a portable air conditioner's cooling output compared to its energy input. Higher CEER is better because it means greater efficiency and less energy use. CEER takes into account the power used when the unit is actively cooling and also when it's in standby mode. The older measure of efficiency is the energy efficiency ratio (EER), which does not take into account the power used when the device is in standby mode.

Heavy-Duty Portable Air Conditioners

Heavy-duty portable air conditioners are sturdily built devices designed to provide easily movable sources of cool air in industrial and commercial buildings. There are two basic kinds of heavy-duty portable air conditioner: air-cooled and water-cooled units.

Air-Cooled Portable Air Conditioners

Heavy-duty air-cooled portable air conditioners work basically the same way as light-duty portable air conditioners. They absorb heat and moisture within the space and transfer it out using ventilated air. Their exhaust hoses can be mounted in windows, or they can attach to ductwork above a drop ceiling connecting to the building's return air plenum. In warehouses and high-ceilinged industrial buildings, exhaust chimneys can conduct the heated air toward the top of the building, where ventilation will allow it to escape.

Some units also have nozzles that allow cold air to be aimed at workstations or equipment for spot-cooling purposes.

Water Cooled Portable Air Conditioners

Water-cooled portable air conditioners transfer the heat that they absorb to water, rather than air. This water carries the heat away from the space. This is the only kind of portable air conditioner that can be used away from windows, ductwork or other ventilation. However, they must be attached to a water source and drain. Water-cooled portable air conditioners are also generally more efficient than their air-cooled counterparts, and more effective at cooling when the temperature is very high. 

Applications for Heavy-Duty Portable Air Conditioners

Industrial and warehouse applications: Portable air conditioners are widely used to cool assembly lines, providing efficient, direct cooling to people working in production and warehouse environments. Portable air conditioners are also useful for cooling industrial equipment, helping to reduce cycle time and prevent premature failure of heat-sensitive equipment in CNC machining, food processing, injection molding, robotics and automated processes.

Information technology applications: Portable air conditioners are widely used to cool sensitive equipment in server rooms, telecom closets, back offices and data centers. Portable air conditioners designed for IT applications often feature advanced remote management tools.

Other common applications for heavy-duty portable air conditioners: Heavy-duty portable air conditioners are also commonly used for spot cooling in health care facilities, schools and universities, sports facilities and temporary structures.

Frequently Asked Questions

Q: Do portable air conditioners need to be near a window?

A: The short answer is that most of them do. The basic function of any air conditioning system is to remove heat and moisture from the air inside a room or building. Most kinds of AC system, including most portable air conditioners, use ventilated air to send away the unwanted heat and moisture. There are some heavy-duty portable air conditioners designed for operation away from windows, but most portable AC units require an exhaust hose to be attached to a window, sliding door or other building aperture. Without a link to the outside, that hot, wet air has nowhere to go.

Q: What's the difference between ASHRAE and SACC ratings for portable air conditioners?

A: The ASHRAE and SACC ratings are both evaluations of portable AC cooling capacity in BtuH. The SACC rating was introduced in 2016 and is lower than the ASHRAE rating for the same equipment.

The information contained in this article is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This article is not a substitute for review of current applicable government regulations, industry standards, or other standards specific to your business and/or activities and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

Featured Resources

SIGN UP FOR EMAIL

Get more great content like this sent to your inbox.

promo

THE PRODUCTS YOU NEED,
WHEN YOU NEED THEM

SHOP NOW