COVID-19 RECOVERY - Products and Solutions to help your business move forward - Learn More

Equipment

Diagnosing Your Power Tools: 5 Warning Signs & What They Mean

11/1/16
Grainger Editorial Staff

Like most heavy-use equipment, power tools fall victim to wear and tear, malfunctions and electrical issues. Even when the best tool maintenance is carried out, tools can stop working and need immediate inspection and possibly repair. If you’ve been on the end of a belt sander smoking or a miter saw squealing, then you know tool malfunction is not something to take lightly.

However, with some careful examination, you can diagnose the cause of the issue and determine the next course of action. Check out these five red flags and how to properly inspect your tools for repair.

Remember, always make sure your power tool is disconnected from the power source before your try to diagnose any potential problems.

1. It Won't Start

If your tools won’t start, it could hint at some larger electrical problems including a short or part malfunction.

  • Start by checking the power switch and its assembly to make sure there is no damage as heat and water damage can be the culprits of a tool that won’t start. Using a multimeter can test the voltage on your tool to assess if power is moving through the cord, switch and to the parts of the tool.
  • Dust and dirt accumulation within a tool and can prevent a tool from working so brushes and springs are where you should look next. Brush channels— enclosures consisting of brushes and springs located at the end of a motor where electricity is routed—can become worn and shorten over time. Check your brushes for wear and replace accordingly.
  • A bad power cord can also stop a tool in its tracks and is a visible issue that can be replaced. Kinks, tears or cuts in cords can stop the flow of electricity to the power switch and can be assessed using a multimeter which will tell you if a wire is broken.

2. Weakened Power

Your tool starts but the power level is so weak that you’d probably be better off with a manual screwdriver. Or handsaw. Or bicycle pump. When your power tools lose their oomph (and it’s not a low battery), the most likely cause are old, worn carbon brushes that need replacing. The carbon brushes are the small carbon blocks that transfer the electrical current from your power source to the tool’s motor itself. These wear out through use. If your tool is losing power and doesn’t have the speed or strength it should, it could be an indicator that it is time to replace these parts.

  • Similar to a tool that won’t start, check your carbon brushes for any heavy wear or signs of damage.
  • If your brushes are clear, there may be damage to your tool’s commutator or the rest of the assembly. Discoloration, buildup and even melted insulation are signs that these parts are the root cause.

3. Burning Smell

Malfunctioning motors tend to give off a very recognizable burning smell when something is wrong. Everything is still spinning but the tool is no longer working, and it just stinks.

  • Diagnosing this smell could change depending on the age, type and design of your power tool. If your tool has a drive belt—like a sander or a planer—that is the first place to check.
  • When the drive belt breaks you will get that tell-tale burning smell, and your tool will stop working even though the motor is still running.
  • For other tools, such as power saws, you may want to check if the capacitors need replacing.
  • It could also just be a case of the tool overheating. Motors generate a lot of heat when in use. If the tool has been running too long or too hard, the tool can overheat and cause a burning smell. For best power tool safety, immediately turn off any power tool that is emitting a burning smell and let it sit for about 30 minutes before attempting to diagnose the problem.

4. High-Pitched Screeching Noise

Using power tools can be pretty loud. However, sometimes a power tool starts making a high-pitched screeching noise, or screaming; that goes above and beyond the loud hum of your electric hammer drill.

  • If your tool starts making this noise, first make sure that it is properly lubricated. Check the manufacturer’s specifications for maintaining your tool to find out the best method to keep your tool lubed.
  • Another easy tip for a squealing tool is to check the gears. If your tool has a forward and reverse control (as most power drills do), your gear switch may get stuck between the gears. Gently move the switch back and forth and try running the drill again.

5. Sparks and Smoke

If your power tool begins to emit smoke or sparks, turn it off immediately. You should never continue using power tools that are smoking or sparking. Set your tool aside and allow it to cool down before attempting to diagnose or fix an issue.

  • Once the tool is cooled, check to see if any dust or debris has gotten into the tool. Sawdust or other particles that frequently fly through the air in heavy work areas can get into your tool’s vent and cause that sparking or smoking.
  • If your tool is free of burning debris, you may need to take apart the tool’s casing and check for heat damage.

Power Tool Maintenance

The best way to address issues with your power tools is to avoid them in the first place. Always check the manufacturer’s recommendations for the best ways to maintain your power tools. Following a regular maintenance plan is usually the best way to head off potential problems before they start. Many common tool problems can be solved with simple checks and adjustments to determine if upgrades are available for your company’s needs.

Sources:

http://www.instructables.com/id/fix/

http://www.toolerant.com/is-your-table-saw-motor-stopping-stinking-smoking-or-silent/

http://home-tools.wonderhowto.com/how-to/fix-power-drill-grinding-noise-and-chuck-problem-382812/