COVID-19 RECOVERY - Products and Solutions to help your business move forward - Learn More

Equipment

The Easy Way to Clean Up and Renew Artificial Turf


Grainger Editorial Staff

The game is over, but the work isn’t finished for everyone. Pom-pom streamers, confetti, sunflower seeds and popcorn litter the battered field turf. Ant hills of crumb rubber sporadically rise above the flattened green fiber, and twigs, leaves and other debris swirl in the wind. Grounds managers are now faced with the task of grooming and preparing the artificial field turf before it is playable again.

While picking up trash piece-by-piece would work, it wouldn’t be time efficient or cost effective. And even after hours of labor, the turf would still be flat and dotted with uneven crumb rubber, posing a safety threat to the players who use the field.

Fortunately, the Parker Estate Master® artificial turf sweeper provides the all-around solution. Used by professionals throughout the country, the Estate Master is the optimal tool for grooming and cleaning artificial turf, as well as for smoothing crumb rubber. Uneven crumb rubber not only can compromise an athlete’s performance but it can also cause players to stumble, increasing the risk of injury.

The Estate Master system is formed by hitching three Parker Suburbanite® turf sweepers together, creating a 100-inch sweeping path. It easily picks up debris like twigs, leaves, trash and items even as small as sunflower seeds. The result is a clean, groomed and safe field. Unlike other sweepers, the Parker Estate Master’s mesh bottom allows any crumb rubber picked up to fall back down and be evenly redistributed onto the field. Evenly distributed crumb rubber is aesthetically pleasing and essential to providing a safe field for athletes of all ages and sports.

Estate Master Sweepers are ideal for managing large spaces, especially artificial turf in football and sports stadiums. Landscape contractors can also benefit from the sweeper, using it to pick up twigs and leaves on natural turf. On natural turf, the mesh bottom allows collected moisture to escape the basket returning water to the grass. The sweeper is easily towed by an ATV with a rear hitch, a front-engine garden tractor or a zero-turn riding mower. Adjustable height and frame options help ensure exceptional performance for varying situations.

David Roundtree, a territory manager for Gardener Incorporated, an outdoor power equipment dealer in Jacksonville, Fla., supplies Estate Masters to grounds managers and stadiums across the United States.

Roundtree compares turf maintenance to taking care of carpet in a home. Both must be cleaned and kept free of debris in order to look good and lengthen their life. “I haven’t seen anything else out there that does what the Parker Sweeper does for the money,” Roundtree said. “It is almost like using a vacuum cleaner at home. Keeping the carpet vacuumed regularly keeps the carpet fluffed up; it’s really no different in this situation.”

So how does the Estate Master create the manicured look? Eight polypropylene, steel-backed brushes circulate through the turf, fluffing the rubber and standing up the blades on artificial fields. The brushes are in four staggered rows and can be adjusted for different heights independent of the frame, ensuring the perfect sweep for every field. Because the Estate Master is comprised of three Suburbanite units, a total of 24 brushes are grooming the field at one time – maximizing performance and efficiency. Each of the three units includes a front face plate with a variable vertical adjustment, as well. Adjusting the height vertically controls how debris is deflected into the basket.

Each unit of the sweeper is constructed for durability. Heavy-duty rear casters, sintered pinion gears and sealed ball bearings on the brush axle help extend the life of the units.

“The construction of the Parker unit is impressive compared to others,” Roundtree said. “The all-metal wheels and gears of the drive system are very durable and can last for many years. Another popular feature is the caster wheels that support the back of the basket. Many low-end machines don’t have any kind of support for the basket.”

The Estate Master’s design and reliability make it a popular sweeper in well-known stadiums throughout the country. Roundtree said several NFL teams use the product, including the Jacksonville Jaguars™ and Tampa Bay Buccaneers.™ Many select university athletic programs also use the Estate Master.

Chad Mixon, grounds manager at Troy University in Troy, Ala., said their program uses the Estate Master exclusively on their artificial athletic turf fields.

“It has been virtually maintenance free,” Mixon said. “We rarely need new parts, and it does what it’s supposed to do.”

The quality of the sweep and its ability to fluff everything up and give the field a manicured look are the best aspects of the Estate Master, Mixon said. “The field goes from a flat hairdo to a teased up hairdo,” he said. It even picks up streamers from pom-poms.  

Whether the debris consists of sunflower seeds or leaves, the Parker Estate Master will sweep away the evidence, leaving only a manicured field and evenly distributed crumb rubber behind.

Article Courtesy of Parker Estate Master

The information contained in this article is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This article is not a substitute for review of current applicable government regulations, industry standards, or other standards specific to your business and/or activities and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

Featured Resources

SIGN UP FOR EMAIL

Get more great content like this sent to your inbox.

promo

THE PRODUCTS YOU NEED,
WHEN YOU NEED THEM

SHOP NOW