What is a Current Transformer?

What is a Current Transformer?

There are more to power systems than meets the eye. In fact, we cannot actually see electricity, but we can see how it works (or doesn’t work). So many elements come together like a puzzle to form electrical power, one of those being a current transformer. Here’s what you need to know about this vital piece of equipment:

 

The Down Low on CTs

A current transformer is a device used to produce an alternating current in its secondary, which is proportional to the AC current in its primary. This is primarily used when a current or voltage is too high to measure directly. The induced secondary current is then suitable for measuring instruments or processing in electronic equipment, which typically needs isolation between the primary and secondary circuit.

This reduction of high-voltage currents allows for a convenient way of safely monitoring the actual electrical current flowing in an AC transmission line using a standard ammeter.

An electrical CT differs from a voltage or power transformer because it consists of only one or very few turns as its primary winding. What also sets it apart from a voltage transformer is that the primary current is not dependent on the secondary load current but instead is controlled by an external load. The CT ratio is equal to the number of secondary turns. This ratio is based on the primary conductor passing once through the transformer window.

Classifications and Types

Current transformers can be classified into two separate groups. The first, a measuring current transformer, is used along with measuring devices for the magnitude of current, energy and power. The other, a protective current transformer, is used along with protection equipment, including trip coils, relays, etc.

There are three basic types of current transformers:

  1. Wound type: consisting of two separate windings (primary and secondary) on a magnetic steel core with different turns, depending on the design.
  2. Bar type: consisting of a bar of suitable size and material used as the primary winding, which is equivalent to a single turn.
  3. Window (toroidal) type: has no primary winding but instead has an opening in the core through which the conductor carrying the primary load current is passed.

Make sure your facility has all of the equipment it needs, including electrical transformers to transmit, distribute and utilize altMake sure your facility has all of the equipment it needs, including electrical transformers to transmit, distribute and utilize alternating current electrical energy—safely and effectively.

Sources:

http://www.gegridsolutions.com/products/manuals/ITITechInfo.pdf

https://owlcation.com/stem/What-is-a-Current-transformer-How-does-it-work

http://www.electronics-tutorials.ws/transformer/current-transformer.html

Pub. 05/2017

The product statements contained herein are intended for informational purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. The information provided herein does not replace the use by you of any manufacturer instructions or technical product manual. W. W. Grainger, Inc. does not guarantee the result of product operation or assume any liability for personal injury or property damage resulting from the user’s reference to any product instructions. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion.