Are You a Machining Guru?

Are You a Machining Guru?

Test Your Mettle with Our Quiz

If you work in the machining field, you’ve probably got all the basics down pat. But what about the more nitty gritty details? Ever executed a fillet? Do you wear jewelry while surface grinding? What do you know about climb milling? Put your machining skills to the test with our quiz.

 

Related Categories
Machining

Machining Supplies

Milling

1. What does CNC stand for?



Correct!
 
Wrong! Correct Answer: Computer Numerical Control
 
2. Machining that adds material rather than remove it is called what?



Correct!
 
Wrong! Correct Answer: Additive Manufacturing
 
3. Grinding is the process of machining round parts on a lathe.

Correct!
 
Wrong! Correct Answer: False
 
4. Which of these machines is used in the hole making process?



Correct!
 
Wrong! Correct Answer: All of the Above
 
5. What machine has you “swinging the head?”



Correct!
 
Wrong! Correct Answer: Milling Machine
 
6. Surface grinder safety calls for _______________.



Correct!
 
Wrong! Correct Answer: Safety Glasses
 
7. What is the process of enlarging an existing hole called?



Correct!
 
Wrong! Correct Answer: Boring
 
8. In machining, what is a fillet?



Correct!
 
Wrong! Correct Answer: A channel or groove in a shaft
 
9. Can wood or plastic be used on a milling machine?

Correct!
 
Wrong! Correct Answer: Yes
 
10. Which of the following is considered a principle machining process?



Correct!
 
Wrong! Correct Answer: Milling
 
 

Pub. 09/2017

The product statements contained herein are intended for informational purposes only. Such product statements do not constitute a product recommendation or representation as to the appropriateness for a specific application or use. W. W. Grainger, Inc. does not guarantee the result of product operation or assume any liability for personal injury or property damage resulting from the use of such products.