Abrasive Characteristics and Types

 

Grainger Editorial Staff

Posted: 8/08/18

 
 
 

Proper metalworking requires the right abrasive. These are minerals (or mineral-like substances) used to shape, grind or cut metal. Using the right abrasive is essential to getting the job done without damaging your surface. Learn about the right abrasive types for your particular surface material.

Grit Size

Grit size is an extremely important characteristic when deciding the right abrasive for your task. The grit size indicates the grade on the abrasive side of the paper. The higher the grit size, the finer the abrasive is. The basic descriptions of abrasive types range from coarse to medium to fine. Here’s basic table of the different kinds of grit sizes.

Size Type
12, 16, 20 Super coarse
24,30,36 Extra coarse
40,50,60 Coarse
80,100 Medium
120,150,180 Fine
220,240,280,32 Extra fine
400,500,600 Super fine
800,1200 and finer Extra fine

SURFACE MATERIAL

Abrasives have multifaceted functions based on their characteristics. For your job to be successful, the abrasive material must be stronger than the surface in which it's applied. Abrasives can be classified into two separate categories: natural and synthetic. Here are some of the most common surface materials and which abrasives to use based on the function:

WOOD

Wood is a very popular surface material that needs manipulating like calibrating, sanding, prepping for polishing, keying and more. For light and small sanding jobs, use the abrasive garnet, which is natural and inexpensive. Garnet typically comes in medium and fine grit size paper.

The best abrasives for smoothening wood are silicon carbide, which is a combination of synthetic and natural materials, and aluminum oxide, a synthetic material. Both come in a wide grit size range based on the fineness of the task.

METAL

Metal can be a difficult material to try and manipulate due to its strength and rigidity. Smoothing this surface requires the use of a tough abrasive, such as aluminum oxide. This abrasive can also help remove paint or rust on metal. To smooth or polish metal, opt for a natural material like emery, which isn't aggressive enough to scratch.

For heavy metal removal, ceramic is the right abrasive for the job. This is a rugged, industrial-duty aluminum oxide that's available in medium, coarse and extremely coarse grits.

STEEL

Steel is a strong, alloy of iron. So for grinding, blending, cleaning or smoothing it requires the use a tough abrasive like aluminum oxide. This abrasive is for general use and maintenance, repair and other operations. With its strength, it can manipulate even the toughest of stainless steel.

By understanding your surface material, you can better choose the right abrasive for the task at hand. Be sure to check out our Blast Media Chart to understand all the different types of abrasives.

SOURCES:

https://knowledge.axminster.co.uk/choose-the-right-abrasive

https://www.fepa-abrasives.com/abrasive-products

http://www.horiba.com/scientific/products/particle-characterization/applications/abrasives

http://www.sigmaaldrich.com/chemistry/stockroom-reagents/learning-center/ technical-library/particle-size-conversion.html

http://www.inclusive-science-engineering.com/types-of-abrasives-products

http://www.mechanicalengineeringblog.com/4836-abrasives-types-of-abrasives

 
 

 

Email Address:  (Required)

Industry:

 

The information contained in this publication is intended for general information purposes. No representation is made that the information or references are complete or remain current. Click here for Grainger's full legal disclaimer.

Have a question, comment or need assistance? Send us a message. We’re happy to help.