Mold Control: Critical Tips on How to Clean Up and Prevent Mold After a Flood

Grainger Editorial Staff

Posted: 6/20/18

Mold Control: Critical Tips on How to Clean Up and Prevent Mold After a Flood

After the hurricane blows through and the heavy rains recede, your problems may be just beginning. Water damage can quickly lead to mold, which poses serious health risks.

These tips will help you start the cleanup effort and prevent mold after a flood.

How long does it take for mold to grow after a flood?

The microorganisms that turn into mold colonies are always in the air around us, so mold growth will start quickly—within 24 to 48 hours of water exposure. Mold colonies will continue to grow as long as the moisture level is high. In buildings, mold is most fond of wood, drywall, ceiling tiles, carpet and insulation.

What’s the best way to prevent mold after flooding?

The only way to prevent mold from growing is to dry the affected area as quickly as possible. To do this, take these steps:

  1. Open up the building if it’s less humid outside. (In general, you’ll want to open the building during the day and close it up overnight.)
  2. Remove all debris and wet items. Clean exposed surfaces with disinfectants or sanitizers.
  3. Get rid of any soaked porous or absorbent material that you can (like ceiling tiles, papers, furniture and even water-damaged drywall, carpeting and insulation).
  4. If you can’t get rid of saturated carpeting right away, remove water from it with a carpet extractor or wet/dry vacuum.
  5. Use fans to circulate air into the space and speed evaporation.
  6. Use dehumidifiers to reduce the moisture content of the air and help things dry more quickly, especially in closed areas. A home and office dehumidifier may be enough for smaller areas, but large spaces and moisture-saturated areas may require an industrial/commercial dehumidifier, or even a specially designed restoration dehumidifier.

How long should I run a dehumidifier after a flood?

If possible, run a dehumidifier until porous surfaces in the space have dried out completely. It can take anywhere from two days to several weeks to dry out a flood-damaged building. Materials like plaster and insulation will take a long time to dry, so it may be better to replace them entirely. Until everything is dry, mold can continue to damage the building.

Low relative humidity is what pulls moisture out of these surfaces, and humidity levels below 50 percent will discourage mold growth. You can use a moisture meter to get accurate readings.

What Kills Mold After a Flood?

The American Red Cross and the Federal Emergency Management Agency recommend these cleaning products for mold and mildew removal:

  1. First choice: Commercial mold and mildew removers
  2. Second choice: Washing soda or tri-sodium phosphate (5 tablespoons per gallon of water)
  3. Third choice: A solution of bleach and water (one-quarter cup of laundry bleach per gallon of water)

Remember to use the appropriate precautions and protective equipment for mold remediation when cleaning with bleach, tri-sodium phosphate or other heavy-duty cleaners.

SHOP RELATED PRODUCTS

Mold Killers and Mildew Removers
Mold Killers and Mildew Removers
Disinfectants and Sanitizers
Disinfectants and Sanitizers
Wet/Dry Vacuum Cleaners
Wet/Dry Vacuum Cleaners
Jobsite and Restoration Dehumidifiers
Jobsite and Restoration Dehumidifiers
 

Sources:

https://www.nytimes.com/2006/07/09/realestate/09home.html

https://www.grainger.com/content/qt-210-mold

https://www.redcross.org/images/MEDIA_CustomProductCatalog/m4540081_repairingFloodedHome.pdf

 

 

 

Email Address:  (Required)

Industry:

 

The information contained in this publication is intended for general information purposes. No representation is made that the information or references are complete or remain current. Click here for Grainger's full legal disclaimer.

Have a question, comment or need assistance? Send us a message. We’re happy to help.