Navigation Menu New

Access My Account, Order History, Lists and more here.

Steel & Beam Anchors

13 products
Steel and beam anchors attach to structural steel (such as an I-beam, H-beam, or pipe) to serve as a tie-off point for a fall arrest device. They are clamped, welded, or bolted in place. They often have a smaller footprint than other connectors and can be used where the mounting point is not fully exposed, such as anchors that clamp onto beams. Fall arrest systems are used when working at height, such as when performing construction and maintenance tasks. Anchors should always be inspected and replaced after being exposed to a fall.
Brand

Sliding Clamp Anchors for Steel & Beams

Sliding Clamp Anchors for Steel & Beams
These sliding clamp anchors attach to structural steel and beams to create a moveable anchor point for a fall arrest device. Sometimes called gliding, trailing, or mobile beam anchors, sliding clamp anchors have two edges that adjust to fit a range of beam widths. They have wear pads, bearings, or materials that allow the anchor to slide along the length of the beam without having to be removed or adjusted, providing greater mobility for workers than fixed clamps. Sliding clamp anchors can be removed and reused in other locations. Anchors should always be inspected and replaced after being exposed to a fall.

Anchor Performance: Unspecified

Loading...

Extended Life

Loading...

General Purpose

Loading...

Smooth Glide

Loading...

Fixed Clamp Anchors for Steel & Beams

Fixed Clamp Anchors for Steel & Beams
These fixed clamp anchors install on beams and other structural steel to create a stationary anchor point for a fall arrest device. They have two edges that adjust to fit a range of beam sizes. A D-ring provides the attachment point. These clamps can be removed and used in other locations. Anchors should always be inspected and replaced after being exposed to a fall.

Anchor Performance: Unspecified

Loading...

General Purpose

Loading...

Rolling Trolley Anchors for Steel & Beams

Rolling Trolley Anchors for Steel & Beams
These rolling trolley anchors have wheels that reduce friction as the trolley moves, allowing workers to move freely without manually moving the anchor. Sometimes called rolling beam anchors or rolling anchors, they adjust to fit a range of beam widths. A D-ring connection point hangs below the trolley to provide an overhead attachment. These anchors can be removed and reused in another location. Anchors should always be inspected and replaced after being exposed to a fall.

Anchor Performance: Unspecified

Loading...

General Purpose

Loading...

Smooth Glide

Loading...

Drop-Through Anchors

Drop-Through Anchors
These anchors have a plate on one end to hold the anchor in place when dropped through a hole in structural components such as steel, beams, and concrete. The attachment point on the other end connects to a fall arrest device. These anchors can be reused and provide a longer reach than D-ring anchors. Anchors should always be inspected and replaced after being exposed to a fall.
Loading...

Clamp Anchors for Steel Pipes

Clamp Anchors for Steel Pipes
These clamp anchors (sometimes called hand grip anchors) close around the circumference of a horizontal pipe or beam. The clamp squeeze open it so it can be placed around the beam or pipe, and it closes automatically when released. The attachment point hangs below the pipe so the worker can make an overhead attachment. These clamps move along the length of the beam or pipe, allowing workers to move freely without manually moving the anchor. They can be removed and reused in other locations. Anchors should always be inspected and replaced after being exposed to a fall.
Loading...

Toggle Anchors for Steel & Beams

Toggle Anchors for Steel & Beams
These toggle anchors are inserted into a predrilled or precast through-hole in concrete. They have a toggle that is pressed to allow the anchor to be pushed into the hole. When the toggle is released, the end of the anchor expands to hold the anchor in place. These anchors can be removed and reused in other locations. Anchors should always be inspected and replaced after being exposed to a fall.
Loading...
Note: Product availability is real-time basis and adjusted continuously. The product will be reserved for you when you complete your order.