Navigation Menu New

Access My Account, Order History, Lists and more here.

Electronic Fluorescent Ballasts

Available55 products
Electronic fluorescent ballasts can replace burnt-out electronic or magnetic ballasts in fluorescent lighting fixtures. They are more efficient than magnetic ballasts and do not hum or cause lights to flicker. These ballasts are compatible with switches, occupancy sensors, and other lighting controls that turn lights on or off but do not dim their light output. Electronic ballasts protect light bulbs from damaging power fluctuations that can reduce the quality of the bulbs' light output. They provide an initial spike of high voltage to turn on light bulbs and then regulate the current to the bulbs for as long as they are on. Replacement ballasts should have the same voltage and start type as the old ballast, be able to power the number and type of bulbs that are used in the fixture, and be capable of fitting into the fixture.
Brand

Instant Start Electronic Fluorescent Ballasts

Instant Start Electronic Fluorescent Ballasts
Instant-start electronic fluorescent ballasts turn on lights immediately and are used in fluorescent lighting fixtures in warehouses and other areas where lights are left on for long periods of time. They provide high voltage at start-up and should not be used with occupancy sensors or other lighting controls that turn lights on or off frequently.
Loading...
Loading...

Programmed Rapid Start Electronic Fluorescent Ballasts

Programmed Rapid Start Electronic Fluorescent Ballasts
Programmed rapid-start electronic fluorescent ballasts turn on lights near-instantaneously. They are more energy efficient and less damaging to fluorescent light bulbs than instant-start ballasts and rapid-start ballasts. They are used in lighting fixtures that will be turned on or off frequently via occupancy sensors and other lighting controls that automatically operate the lights. The ballasts provide a small amount of voltage to preheat the bulbs' filaments before the bulbs turn on. This small initial voltage is supplied for a specific amount of time to avoid glow current, which can damage the light bulbs.
Loading...

Rapid Start Electronic Fluorescent Ballasts

Rapid Start Electronic Fluorescent Ballasts
Rapid-start electronic fluorescent ballasts turn on lights near-instantaneously. They are less damaging to light bulbs than instant-start ballasts and are used in lighting fixtures that will be turned on or off frequently via occupancy sensors and other lighting controls that automatically operate the lights. The ballasts provide a small amount of voltage to preheat the bulbs' filaments before the bulbs turn on.
Loading...
Note: Product availability is real-time basis and adjusted continuously. The product will be reserved for you when you complete your order.